Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear Support Team,I have problem with STM32F105RBT6 overheating,After several months of operation, the processor will break down, overheat and burn out completely.Power consumption is constantly rising, but it works flawlessly even with higher power ...
Hello, I have some project with RTC. Initially project was made with STM32F405 uC, now all porting to STM32F765 uC. Problem with RTC, on the new board with F7 uC I have error around 2 sec per day, where board f405 - I have error 1 sec in 4-5 days. B...
I did a fresh install of STM32CubewMX and STM32CubeIDE. I built a simple program that does nothing except configure an LED to turn on as part of the GPIO initialization. Try as I might, I can program it when trying to debug, but cannot debug. Excerpt...
Are there daughter boards available for eval board to buy?According to user manual um2198, Two 40-pin male headers CN11 and CN12 are used to connect with memory daughterboard.Two 60-pin male headers CN6 and CN7 can be used to connect a daughterboard ...
Anyone know the whereabouts of a new or used STLINK V3SET programmer tool in North America?None of the usual disty suspects have any. All are backordered.No wisecracks, please, about why one needs a programmer/debugger when you can't buy any parts t...
Anyone know the whereabouts of a new or used STLINK V3SET programmer tool in North America?None of the usual distribution suspects have any. All are backordered on this item. Even Asian distributors are out.
Hello,I'd like to erase and load an hex file on a STM32 without use the STM32CubeProgrammer as interface. Is it possible integrate the ST-LINK v2 (SWD interface) functionality in a python/C# script to automatize the erase/flashing and integrate it w...
After this second trial, the only way that I'm able to program the MCU is using the JLINK, but I would really need the STLINK-V3MINI working as expect.
I am using STM32CubeIDE V 1.9.0, with an Nucleo board with STM32F401, and STLink integrated. Debugger just stopped working. I have spent hours trying to change debugging configurations, upgrading STLink firmware, but nothing. When I press Debug I see...