I'm using a Nucleo-F746ZG with timer 2 as a quadrature encoder input. I'm feeding it quadrature signals from 2 GPIOs at 250Hz (each phase is 1mS).The CDR value is 0, so FDTS should be CLK_INT (36MHz for APB1). With both inputs' filter set to 8, the...