Associate II
July 6, 2021
Question
Power management issue STM32L078RB
- July 6, 2021
- 2 replies
- 1088 views
I join the schematic of my board to the question.
I am unable to connect my custom board, the error message on STM32CubeProgrammer is "Not STM32 target found" even it detects the supply voltage. The VDD required for the MCU is 1.8V and I connect all supply input pins to VDD. I also placed decoupling capacitors close to these pins. I have no idea why the MCU doesn't start.
Any help or suggestions to check is welcoming