User Activity

Hi everybody,I am currently working on a project with a BlueNRG-M2 module running the DTM firmware to get interfaced by an host controller.The Project requires lots of parameters to send and receive via BLE and my device is in client role. While addi...
Hi everybody,I'm using the BlueNRG M2 module on a custom hardware with a separate Host controller. It is a battery driven device so the power consumption should be as low as possible when BLE communication is not needed. The Application Note AN4820 d...
Hi,I'm using the BlueNRGM2 BLE module in combination with a STM32L4 host controller. They are connected over SPI.The BlueNRGM2 is running the DTM_SPI application from ST to act as network coprozessor. My user application is running on the host contro...
Hey guys,I try to connect a NUCLEO-F429ZI board with STM32CubeIDE.I have first installed the latest version of the IDE on an Windows 10 machine with the ST-LINK USB drivers that are required. When I know try to run or debug a simple example project t...
Kudos from