STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

POST REQUEST AT COMMAND ESP 8266

HIPLEASE I WANNA OPEN A HTTP POST REQUEST TO POST DATA ON A LOCAL SERVER CONFIGURED WITH SPRING BOOTI AM USING ESP8266 AT COMMAND AND I ALREADY OPENED A TCP CONNECTION YET POSTING THE DATA ON THE DATA BASE IS NOT WORKINGAM USING THIS COMMAND char req...

atoua.1 by Associate
  • 1397 Views
  • 1 replies
  • 0 kudos

Program STM32F103C8T6 with USB

Hi everyone, I want to program using the usb connection on the STM32F103C8T6 board. There are examples using Arduino, but it cannot perform STM32 functions.How can i program via usb and look at sensor data?  I need help. Thank you from now

EDT Graphich Display with STM32F7 MCU

Hi guys,I'm working on a Projekt, that it should be STM32F7 interfaced with a EDT-Display but without using the Operating System or TouchGFX.The Developer had designed the Board in a way, that nobody can use it directly without FreeRTOS or TouchGFX.I...

mids400 by Associate III
  • 2260 Views
  • 1 replies
  • 0 kudos

Resolved! STLINK-MINIE SWD not working

Hey guys,I have nucleo and STLINK mini boards that I can upload programs into my custom boards with STM32. But I decided to buy the new STLINK MINIE.When I try to connect some board with STM32 (custom board or nucleo), using STLINK-MINIE, I get this ...

2023-07-03-10_41_06.png
MRebo.3 by Associate II
  • 5983 Views
  • 6 replies
  • 0 kudos

STLink-V3 MiniE return DEV_TARGET_CMD_ERR

Hi,I'm using STLink-V3 MiniE tu flash STM32L432CCU6 on custom board.The signal mapped are SWDIO & SWCLK. I connect T_VCC to 3V3.The connexions are correct has I was able to flash the target.I'm using STM32CubeProgrammer CLI, and control the target po...

ABric.2 by Associate II
  • 1696 Views
  • 1 replies
  • 0 kudos

Bluenrg 232 power management

HelloI have a custom designed circuit with bluenrg232 soc. There is a capacitor connected to Vin. Our problem is that the circuit works at the first start but when I turn off the power and wait for 10 or 20 seconds, I start it but now the circuit doe...

MustafaE by Associate
  • 943 Views
  • 0 replies
  • 0 kudos