2025-05-03 9:20 PM
Hi there!
Im new with ST MCUs and im using a Nucleo F429ZI, i have some documents and one of them is the 'nucleo-f429zi.pdf' but is too short and doesnt have too much information
Im working with user push button connected to PC13 but i want to know if this button has an external pull up/ pull down resistor on the board, and if doesnt i guess i have to set it by software
Where can i found schematics or additional information like this for this board?
Also you would help me if you tell me if PC13 has a pull up/down resistor on the board
Thanks in advance!, sorry for my english, not a native speaker
Solved! Go to Solution.
2025-05-04 3:39 AM
With the STM32 devboards, you can always find their schematics under "CAD Resources" of their webpage, e.g. for the Nucleo-F429ZI (which btw. is obsolete in favour of Nucleo-F439ZI, which is identical except the 'F439 has enabled the crypto features) here.
JW
2025-05-04 3:39 AM
With the STM32 devboards, you can always find their schematics under "CAD Resources" of their webpage, e.g. for the Nucleo-F429ZI (which btw. is obsolete in favour of Nucleo-F439ZI, which is identical except the 'F439 has enabled the crypto features) here.
JW
2025-05-04 8:21 PM
Thanks man!, im new to ST so this kind of stuff is not as clear to find for me
2026-06-01 12:17 PM
What CAD format are these schematics in?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.