Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello STM Community,I currently have a NUCLEO-U575ZI-Q board and the X-NUCLEO-IKS4A1 motion MEMS and environmental sensor expansion board. I’m looking to add BLE functionality and was considering the X-NUCLEO-WB05KN1.Before proceeding, I’d like to as...
I have designed a STM32H723 board with LAN8742A PHY IC and its connected to a Hanrun HR911105A Magjack. I am running the Ethernet stack on mongoose network library. The stack is working perfectly on a STM32H7 Nucleo Board, the link auto-negotiates to...
Hello, I have a Nucleuo-F767ZIT6 board on which I verified a Ethernet code using FreeRTOS in Netconn API, there the code works fine without any issues. So, I moved on to designing a custom board for the same controller the first board worked without ...
Hi STM Community, I’m currently working with the NUCLEO-G491RE board and need some guidance regarding DFU (Device Firmware Update) mode. According to the documentation, CN2 is marked as the DFU connector. Based on that, I have soldered 4 pins on CN2....
I am using an STM32H755ZQ device and unable to start a debug session using STM32CubeIDE + ST-LINK (SWD).The system uses two STM32 controllers, where firmware is flashed to one controller and data is shared/communicated to the second controller.Debug...
Hello,I’m working on a project with the NUCLEO-H753ZI board and need to connect multiple devices. I’d like to know:1. How many GPIO pins are 5 V-tolerant for digital input?2. How many GPIO pins are available for general use, both 3.3 V-only and 5 V-t...
Hello STM Community,I am facing a GPIO output issue on the STM32 NUCLEO-WL55JC2 board and would like some clarification.Test case:I am using the following line of code to set a GPIO pin HIGH: HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); // ...
Hello,I want to use the STLink-V3PWR and OpenOCD in SWD mode. I can just use hla_swd as transport and not SWD otherwise I will get the error "Debug adapter doesn't support 'swd' transport". Is there no possibility to use SWD?BR
Hello everyone, I've finished my project with STM32WBA55 and now I'm going to design a small circuit board. I'm using Altium Designer. I can't access the CAD files for Nucleo WBA55. Can you help me? I don't understand if St.com has changed or is no...
Hello forum,I'm designing for my company a very-low-cost parallel (10 tap) programming tool for STM32F4 target. The solution identified is an SBC with an isolated usb hub where 10 STLINK-V3MINIE are installed. Actually we've successfully tested this ...