Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I am trying to operate NFC IC ST25R95 on a custom board. But I can't get any answers. I attached a logic analyzer. To validate the circuit, I connected the SPI lines to a Nucleo-f413zh and ran the example code from the X-NUCLEO-NFC03A1 library...
Hiii everyone!!!! i want to use ADXL345 as accelerometer by using spi communicatiton and debug and display the value of respective axis in any serial monitor. Please give me the respective code for my guidiance.
I tried to reset the DFSDM1 Peripheral for two days using the STM32H7A3ZI and STM32Cube FW_H7 V1.11.1 (If that's important)I want to Change OversamplingRatio and RightBitShift during the run of my program.Apparently you do this by calling: MX_DFSDM1_...
We are looking to work with the STM32U5A9J-DK Discovery kit, which features the STM32U5A9NJH6Q MCU. Our application requires the use of the Octal SPI flash memory in a FreeRTOS environment. Specifically, we need to perform simultaneous read and write...
Hi Community, I have recently purchased Nucleo H7A3ZI board and while trying to connect through Stm Cube Programmer i have found that it is not detecting target itself. What is possible reason for this? 1. Port is getting detected in laptop2. Stlink ...
it's been week since I stuck on this problem, I have a board like this , SPI3 MOSI PB5 is connected to ic 74HC594s to drive LEDs, and MISO PB4 is connected to 74AC165D to get the four SW (buttons) for input purpose, and the PB3 for clock on both ICs....
is there anyone who worked with the MB1400 Wi‑Fi module or has an idea about it? I'm working with the STM32H7 Nucleo-144 board and I need to add a Wifi module, I find a problem when connecting the module to the card I can't understand how to match th...
i am using STM3210E Eval board which has STM32F103 uC i am trying to recorded some adc value over the period of long time but with the time. I am using RTC to achieve that so that even in case pf power loss the adc might not get measured but the time...
Hi I am using Nucleo H7A3ZIQ board. I want to generate two sine waves of different frequencies on the DACs of the board. I followed the instructions from this youtube video link https://www.youtube.com/watch?v=6Z1L6ox63j0. I was able to generate sine...
Hi, I want to connect an external RAM through the FMC interface to my STM32H753ZI controller. I am making a board that is adapted to ZIO connectors in the KICAD software and the problem is that PIN PF12 can only be connected from ST morpho connector ...