STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Load external flash from command line

I have an STM32H7B31-EVAL board setup with TouchGFX.  I am able to compile and load a project using STM32CubeIDE.  I would like to be able to do the same from the command line.  I found this document that gives a very basic outline of the STM32_Progr...

AQue by Associate III
  • 2907 Views
  • 2 replies
  • 2 kudos

Resolved! Evaluation Board for STM32H725ZGT3

Hi,I have evaluated various controllers and found that the STM32H725ZGT3 is the best fit for our product due to its memory (both NAND & RAM) size, operating temperature range, secure boot hash features, and ECC capabilities. However, I am unable to l...

Unable to get data from IIS2ICLX.

HelloI have a P-NUCLEO-WB55-NUCLEO attached to a X-NUCLEO-IKS02A1 attached to a STEVAL-MKI209V1K. I am trying to measure tilt using the some of the same hardware as shown in this ST video. When I run my application (which I have attached to this post...