STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Short-circuit on STM32H743

Hello!I've been working with several STM32 parts since 10 years. I'm working for a company so due to confidentiality I can't share the schematic of the custom PCB, sorry.On the first batches of a new product, using a STM32H743BI, it appears that some...

jean by Senior
  • 3364 Views
  • 5 replies
  • 0 kudos

STM32L4P5G-DK Clock Config Error

When I try to run code using the default clock settings sometimes I get an error at the line:if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){Error_Handler();}I'm confused because sometimes I get an error here and sometimes I do not and nothing c...

sarahsd0109_0-1734200568816.png

Resolved! Problem with USB_OTG again

        Dear helpers,Thanks to valuable assistance from members of this forum I managed to get my project running on a STM Nucleo-H723ZG board, even with a USB-OTG connection to a VCP on my desktop PC. There is only one issue with this connection I c...

FredS by Senior
  • 1212 Views
  • 1 replies
  • 1 kudos

Programming stm32f103 troubleshooting

Hello, the reset pin of the stm32f103 chip I use uses this method to limit the current and pull it up, but there is a phenomenon that the chip cannot be programmed normally. After checking. The reset terminal potential is about 1.23V. The chip can be...

JACK8 by Associate
  • 2432 Views
  • 4 replies
  • 3 kudos