cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Nucleo support for 1.8V

smul
Associate

Hi

I'm using the STM32H755ZI board which has the option for 1.8V DVDD (using JP5).

Does switching DVDD to 1.8V from 3.3V limit the functionality of the board in any way ?

Are the interfaces (CAN, I2C, SPI, UART etc) still functional at 1.8V ? 

Thanks in advance for any help

1 REPLY 1
Uwe Bonnes
Chief

Have a loo at the datasheet

5.3
Operating conditions
5.3.1
General operating conditions
E,g,USB needs 3 V minumum