STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing IRQ Handler for Analog watchdog

Hello,I have an STEVAL-ESC001V1 board and I want to drive a motor in "6-Steps" mode. I have generated a project using MCSDK 6.3.0 version. When I download the code to the board, it is connected to Motor Pilot. But when I send the "Start" commands, no...

Motor Control Support

Hi,We are using STEVAL-SPIN3201 to evaluate STSPIN32F0 which we are planning to use in one of our motor driver.We have 24V, 60W BLDC motor of max. speed 1500 rpm and trying to drive/control it using MC Workbench of MCSDK-6.3.0 in FOC mode.We need som...

Pilot.png Control_Modes.png Profiler.png

Operating BLDC motor in Speed Control Mode

Hello!We are trying to run the BLDC Motor (BL34E34-01) in speed control.A project was previously shared with us that allowed us to run the same motor in position control mode. Given a target position and duration, the motor reaches the final position...

JAM_1999 by Associate
  • 147 Views
  • 1 replies
  • 0 kudos

MC 6.3 with MX6.12 - attr not supported : Dmpu

I am trying to generate code for "STM32 Nucleo packs FOC and 6-step motor control platform for three-phase, low-voltage and low-current motor" and I keep getting errors :-Attr not supported : Dmpu  as in attached image. I am using cubeMX12, I have up...

mc.JPG
Sujoy_B by Associate II
  • 1205 Views
  • 15 replies
  • 1 kudos