build error
I got error mentioned below. How to resolve it. I am using x-nucleo-ihm08m1 with STM32f303re control board for six-step
I got error mentioned below. How to resolve it. I am using x-nucleo-ihm08m1 with STM32f303re control board for six-step
Hello, I put all values of pole pair speed current etc as show in below screenshotbut while during i start the profile speed feedback error i getplease let me know what is the problem
How to find the value of Rs, Ls and B-emf constant and sensor displacement , placement electrical angle please let me know as soon as possible
It would be very useful to be able to use an external encoder using any serial protocol.I'm working with a RLS AksIM-2 with SPI, and I don't see an easy way to integrate this encoders with the code generated by the MC Workbench.As at the moment the o...
Hi, I was trying to use Profiler in Motor Pilot to find motor settings for the evaluation board (ESPIN32F0602S1). However, I found out that the current version of Pilot (V1.2.4 from MC Workbench V6.2) didn’t support the evaluation board (ESPIN32F0602...
In your last webinar about the 6.2 release of the STM32 Motor Control SDK I asked about this and I got the next reply:No native support is planned for SPI encoders. However, we have many customers doing this very thing. The FOC Scheme needs position ...
When I try to set all details into the Motor Control Workbench (with Hall Sensors) at Motor Parameters, there are fields for Inertia and Friction, that I am not sure how to configure.The motor spec is as below images. What should I set for Inertia a...
Version: MCSDK 5.4.8 / MCSDK 6.2.0Tool: Firmware / MC WBEvaluation Board: IHM042-V1Details:When using MCSDK 5.4.8 I am unable to have the first motor perform in the same manner as the 2nd motor despite all parameters being identical and the same mot...
Hi,I have a Nucleo-F302R8 and a Steval-IPM10B, and I would like to configure speed control using UART communication. I have connected an external ARM Cortex-M4 to communicate with the Nucleo to control the speed. Could you please suggest a library or...
Hi all,I need to insert fault on upper key of the driver. In order to achive this Im changing dedicated TIM1 output to Input to output low. After inserting fault motor stops. Is it possible to achive this? Could someone explain what Im doing wrong. ...