STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NetXDuo custom phy interface

HelloI have STM32H563 with KSZ8081 ethernet phy. On FreeRTOS + LWIP i was able to define the PHY in CubeMX and it was basically working out of the box. However on the NetXDuo when i select Custom Phy Interface I am a bit lost. Are there any guideline...

X-CUBE-CELLULAR for STM32H5

Hello,I am currently engaged in an IoT project utilizing the STM32H5 microcontroller unit (MCU). I would like to inquire whether the X-CUBE-CELLULAR library is available for the STM32H5 MCU. If it is not currently available, are there any plans to po...

Egemen by Associate II
  • 173 Views
  • 1 replies
  • 0 kudos

Resolved! a bug about using execution profile kit in threadx

Hi, i'm trying to use execution profile kit in threadx. I use STM32H750VBT6 and STM32CubeIDE1.12.0firstly, i use stm32cubemx to generate the code include threadx. I can't find execution profile file in the code. So I get tx_execution_profile.h and tx...

xixi by Associate II
  • 351 Views
  • 4 replies
  • 2 kudos