SIL3 certified (functional safety) MCU
Hi team,Looking for functional safety complaint MCUs.Kindly Suggest SIL3 certified MCU's which would be helpful for designing.
Hi team,Looking for functional safety complaint MCUs.Kindly Suggest SIL3 certified MCU's which would be helpful for designing.
Hi,I'm using stm32f103vet6 in my design, but due to the limit power budget, the MCU consumes much power(60mA per MCU , while I used 2 chips in my design), result in frequently triggering over current protection. Is there pin to pin compatible STM32L ...
Hello, I'm attempting to establish communication between an STM32L552CET6 microcontroller and an external flash memory. When I manually initiate communication, the component responds to the microcontroller, indicating no hardware issues. However, whe...
Hello all,I'm using STM32L552 MCU and its I2C peripheral to control a board. I'm facing a phenomenal which I not quite sure how to handle that. I have a pretty old fan controller chip on the board which is kind of really slow. Not only it works with ...
I have a custom board using the STM32L562Q BGA package processor. I have a high speed capable eMMC part with an 8-bit data interface. The STM Cube generated code seems to be correctly beginning the init and ID process, however after the 3 different ...
Hello everyone,I have been using for a long time the stm32L496ZGT6 in a customized PCB with an uSD card module. Never had any problem interfacing the card. Due to the shortage of supply during the pandemic situation I bought a couple of stm32L552ZET6...
I am wondering if anyone notice that FDCAN on STM32U5 and STM32H5 MPUs has FIFO/queue size limited to 3 (three!) elements only.AN5348 - FDCAN peripherals for STM32 product classes does not mentioned that anywhere. The max FIFO/queue size discussed in...
Hi. I am testing flash read and write operations.In the main function, when I write 1 to address 0x08006000, I can correctly read back 1. However, when using FreeRTOS and performing the same operation within a task, I read back garbled values (such ...
I am using MX25 NOR flash memory 256Mbit (https://www.mxic.com.tw/en-us/products/NOR-Flash/Serial-NOR-Flash/Pages/spec.aspx?p=MX25L25645G&m=Serial%20NOR%20Flash&n=PM2075#Technical-Documents) and I am mounting a littleFS file system on it. The memory ...
Hi everyone,My bootloader is located at address 0x08000000,MEMORY{RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 8KROM (rx) : ORIGIN = 0x08000000, LENGTH = 32K}#define VECT_TAB_OFFSET 0x00000000Uand the app is at 0x08008000.MEMORY{RAM (xrw) : ORIGIN = 0x2...