STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SysTick Callback not being generated?

Hi,I am using a STM32C031G6U6 and I would appreciate some clarification regarding HAL timebase and SysTick timebase selection.I want to use SysTick as a 1ms interrupt so in CubeMX I selected SysTick as timebase (see screenshot): None of the other tim...

Ricko_0-1770359921026.png Ricko_1-1770360000600.png Ricko_1-1770361629621.png Ricko_0-1770361610071.png
Ricko by Senior III
  • 33 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H7 - USBX RNDIS - USBD_RNDIS_EPINCMD_ADDR

Hello,  I'm using STM32CubeIDE 2.0.0 + STM32CubeMX 6.16.1 + FW_H7 V1.12.1 I have a problem with USBX RNDIS.The generated code on file ux_device_descriptor.h  at line 308 is: #define USBD_RNDIS_EPINCMD_ADDR 0x81U In the exemple code of STM32H735-DK fi...

Dams by Associate III
  • 56 Views
  • 6 replies
  • 0 kudos

SDRAM on the STM32F429I-DISC

Hi,I want to fly the STM32F429I-DISC with the 8 MB SDRAM. I use CubeIDE and selected the right board. All units are set to default. I commented out everything that had to do with os.With help of ChatGPT I hacked together an initialization of the SDRA...

DetlefS by Senior
  • 120 Views
  • 5 replies
  • 0 kudos