STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TFT Library.

I have start to interfacing a TFT module which have RA8875L3N driver .Please share its library (API) if anybody have its library or anybody had work on such series of LCD DRIVER.

LACTIC by Associate II
  • 598 Views
  • 0 replies
  • 0 kudos

Interfacing 2 cameras with an STM32

Hi!I need to interface 2 VGA cameras with an STM32. The cameras are for snapshots only, so FPS and throughput are not issues, the only issues are:physical interfacingkeeping up with received snapshot dataretaining the data before storageThere doesn't...

ISeed by Senior
  • 3182 Views
  • 8 replies
  • 0 kudos

how to External QSPI Nor Flash download Image?

I built a Custom Board based on the STM32F769I-Discovery Board.The other major part is the connection Pin of the QSPI Nor Flash.Could I most easily download the image of TouchGFX to QSPI Nor Flash?How do I download a HEX file that contains a combinat...

ikassma by Senior
  • 2650 Views
  • 8 replies
  • 0 kudos

STemWin stops working after 20 ms

I am using the STemWin BASIC_HellowWorld Application.I modified the source code to look like this:void MainTask(void) { char counterstring[128]; int counter = 1; GUI_Clear(); GUI_SetFont(&GUI_Font32_1); while(1) { HAL_Delay(1); ...

MPlan.7 by Associate III
  • 695 Views
  • 0 replies
  • 0 kudos

Resolved! Clarification on model::tick

Am I correct in thinking that if I can only make changes to screen widgets from within the model::tick() function?I had passed the model pointer out to the remainder of my hardware app so it could push new updated data as it happened, but even though...