STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible that Cipher acceleration hardware module of STM32F756ZGT6 changed somehow from one shipping order to another ? Or maybe there are more recently or better files?

I have been using HAL library of cipher acceleration hardware before on the same mcu (first 100 units) without any problems, but in my last order, all mcu goes to hardfault error when i used exactly the same code on it (same binary file). By debuggin...

fosor.1 by Associate
  • 1463 Views
  • 1 replies
  • 0 kudos

Resolved! X-CUBE-SBSFU with third-party firmware

Hi all--I am working on a project using the STM32WB55. I would like to distribute an "official" firmware, but also allow third-party firmware to be installed. The intent is that the official firmware will be open source, so users can make changes to ...

crwper by Senior
  • 4036 Views
  • 9 replies
  • 0 kudos

stm32l562 secure fault occurs when running NUTTX

Nuttx operating system with stm32l562 board, compile the bin file of the board, and then according to the board directory, readme.txt in the operation through the TFM load the bin run, will give the following secure fault problem:[Sec Thread] Secure ...

星周.1 by Associate II
  • 1176 Views
  • 0 replies
  • 0 kudos

Have the scripts included in the MOOC's package changed?

Dear Sirs,I have downloaded and installed thepackage. I am able to build the example projects with CubeIDE flawlessly butthe batch scripts (.bat) are not working. running the scripts(e.g.02_01_Postbuild_SimpleAppV1.bat) I get the error "The specified...

CCatt.2 by Associate II
  • 1677 Views
  • 2 replies
  • 0 kudos

Firmware download via Y-Modem crashes with the following error when selected in UserApp example project "!!Error during file download!!".

Hello guys I hope you can help me with my problem regarding my adaptation of sbsfu.I'm currently adapting the stm32f413h-discovery example project on a stm32429zi. Everything works fine with one mayor exeption. I have difficulty downloading a new fir...

_legacyfs_online_stmicro_images_0693W00000bj8nsQAA.png _legacyfs_online_stmicro_images_0693W00000bj8oWQAQ.png