STM32 MCUs Security

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Support required with SBSFU Implementation on STM32WB55

Hello ST Community,I'm currently working on a project using the STM32WB55 MCU and am in the process of implementing Secure Boot and Secure Firmware Update (SBSFU) in my custom application. As part of this, I decided to test the existing 1_Image_SBSFU...

Sjain_0-1719740326469.png Sjain_1-1719740338555.png
Sjain by Associate III
  • 282 Views
  • 6 replies
  • 0 kudos

STM32WB55 CPU2 HardFault for unknown reason.

Hey guys, how are you?It's been a long time that i'm facing a issue with STM32WB CPU2, most of the times i just fix it without really knowing the cause of it. Basically what happens is after power-up CPU2 simply won't initialize on the first try. I h...

0693W00000Y8ZSRQA3.png 0693W00000Y8ZTjQAN.png
MBuen.1 by Senior
  • 2561 Views
  • 14 replies
  • 0 kudos

BLE ER key and IR key

I see that those keys are hardcoded in the code. As I understand they are responsible to LTK and CSRK.Should I change ERK and IRK between devices , so they are not the same? Asking for security reasons.

DS.4 by Senior II
  • 309 Views
  • 1 replies
  • 0 kudos

Resolved! Hardware Semaphores for SBSFU in STM32WB

Hello guys,I've implemented SBSFU along side with an USB standalone loader for my project using a STM32WB. My question is, should i implement hardware semaphores and shci_notification for CPU2 during flash erasing and writing operations on my USB ext...

MBuen.1 by Senior
  • 417 Views
  • 2 replies
  • 0 kudos