STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Import Elliptic Curve Keys From .pem Files

Hi, I am coding on the NUCLEO H753ZI board with the pack for embedded cryptography (x-cube-cryptolib-3.1.2). While this folder provides example with hardcoded keys, it does not provide an example with keys imported from a file. Typically, I would lik...

EBonv by Associate III
  • 1362 Views
  • 2 replies
  • 0 kudos

STM32CryptographicV3.1.1_STM32H7 and RNG

Hello togetherI use the following library to create random numbers:- LibraryThe sample project runs on my NUCLEO-144 H743ZI. The problem is that the same byte array (RandomString) is generated at every time. *****************************************...

CRC generation while generating binary file

Hello All,We have designed a Custom Board with STM32F777 MCU chip and are using Atollic Truestudio with ST Micro's CubeMX for development.I have implemented a USB boot loader for the same hardware which is working fine with the Custom Board.Now i wan...

Resolved! Access request to X-CUBE-SBSFU package

Hi,I requested a download access to X-CUBE-SBSFU firmware about two weeks ago but I didn't get a reply yet. Is there something else I should do ?

NaviR by Associate
  • 1238 Views
  • 2 replies
  • 1 kudos

Version 2.2 bug 'mergesbsfu' bug

Hi,Upgrading to version 2.2.0 i get this error using the option " --mergesbsfu" (Add a binary header and a sbsfu segment to an elf file):arm-none-eabi-gcc -o "STM32F769I-Discovery_AWS.elf" @"objects.list" -mcpu=cortex-m7 -T"../STM32F769NIHx_FLASH.l...

Hardware accelerated Crypto: AES CTR mode

I am using multiple MCUs: STM32F733, STM32L433, STM32L443.In STM32CubeExpansion_Crypto_V3.1.0 I am using the software AES CTR encryption (Inc/AES/CTR/aes_ctr.h). I use AES_CTR_Encrypt_Init / AES_CTR_Encrypt_Append / AES_CTR_Encrypt_Finish methods. Th...

NDefr by Associate
  • 1161 Views
  • 0 replies
  • 0 kudos