Resolved! X-CUBE-CRYPTOLIB V4 documentation
Hi,Where can I find a documentation for the version 4 of X-CUBE-CRYPTOLIB ?Regards,Fred.
Hi,Where can I find a documentation for the version 4 of X-CUBE-CRYPTOLIB ?Regards,Fred.
If LL_CRC_INDATA_REVERSE_WORD is set and 8-bit data is provided via LL_CRC_FeedData8(), the resulting CRC is not what is expected. It appears the combination of word-reversal and byte-submission mangles the submitted data in some way, when I had expe...
We are working on developing a host-module that requires two-way device authenticationThe controller we are planning to use is the STM32WL55 Series.We have the following Queries.1) Does STM32WL55 has a functionality to locally generate a certificate ...
I've found an inconsistency between different reference manuals of STM32 embedding the CRYP peripheral, about the management of IVs in GCM mode:The HAL seems to implement the second solution.Could you confirm ?Best regards
In some ST documents the STM32L0X1 is listed as having an RNG peripheral and older versions of the CMSIS headers list the RNG register addresses. Moreover, enabling the peripheral and using it appears to generate random numbers. However newer manual...
Hello,So I'm using a Nucleo-H753ZI (so STM32H753ZI) and I am trying to implement manually (aka without using the HAL library you provide) some drivers of the CRYP module. More precisely, I need to use the CRYP module with AES in counter mode (AES-CTR...
Does the controller perform a CRC confirmation check before running the application to check if the firmware is corrupted? If so, where does this happen; in the bootloader or the application itself? What does it do if the CRC turns out to be wrong? S...
Hi all,I am not sure if I understood the reference manual right: When I activate Read Out Protection RDP Level 1, I can no longer access RTC Backup registers if I execute in RAM. I did not read that also Backup RAM is inaccessible. But it looks it i...
HelloI'm starting to implement AES-GCM on STM32H753 (rev V).I've found an inconsistency between the HAL and the Ref Manual.The STMicro HAL for AES for STM32H7x3 is setting some bits called NPBLB in CRYP_CR register if the product revision is above re...