Hi, team.Question about security of the MCU.Is it possible to log illegal access by the debugger in the state of RDP Level 1? Any bits is a available for it?
Hi ,I am working on STM32U575 nucleo board .Flash got locked (code freeze) and i have to power cycle board to run my application in below cases :Switching from RDP0 to RDP2 in firmware on Pushbutton operation . Application freeze . It runs again when...
WIth oocd I try to do following steps:1) Send reset and halt command2) disable bit DHCSR.C_MASKINTS3) Enable interrupts into ISER reg4) Make any interrupt pending in ISPR reg5) Perform Step commandif readout protection is diasabled, core interrupt oc...
Hello, Having an issue with STM32G031K6Ux MCU. Below added function that checks Options bytes, and if needed - makes changes (power re-cycle is needed after it).This function CheckOptionBytes() works OK on several MCU's. But on this MCU we have an is...
Hi,We are currently using an stm32l5 in our product and experimenting with a stm32L562E-dk and with the official TFM (https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git master branch on the latest commit at this date.) The TFM is unmodified...
Hi,I am facing some issues with debugging SBSFU project.When I flash the application in debug mode, I can not jump to breakpoints set in SBSFU projects.Is there any way to perfrom this.Best Regards,Ankush Nagaraju
I have a workspace in CubeIDE that has two STM32F0 projects: A bootloader and an app.To be able to debug both, bootloader, and then jumping through to the app code, I made an additional Debug Configuration where I added the source folder, and the sym...
I write an application with FreeRTOS using STM32CubeIDE. Now I want to run it as an application with SBSFU. It seemed to have a hard fault after SFU_MPU_SysCall(). My application is a bit big. Its .sfb is 300KB. But it can run correctly alone wit...
I am genreating a hex file from .elf in post, and adding crc to it. Is there any way to debug using new hex, in cubeide 1.1.0