STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CRC-16-IBM using HAL APIs

Hi community, I am working on CRC generation with polynomial 0x8005 and initial value 0x0000, so I configured it as belowI am using the data as shown below and the CRC should be 0x43B8 but the value got from the API is different. So I am missing some...

_legacyfs_online_stmicro_images_0693W00000bkgUXQAY.png

How to Lock STM32L5

I am using STM32L5, In our project, we want to create one script which will lock the bootloader option and enable RDP to 0xCC to disable JTAG.We are using the SBSFU example as a base and developed our application on it.In script Regration.bat, 0xAA R...

PYada.1 by Associate III
  • 2855 Views
  • 3 replies
  • 0 kudos

We use STM32L051C8T6 for mass production.STM32 has been programmed with an hex files. But it was found be locked and we cannot upload new files into them. Who know to unlock the chips?? Urgent!!!

We are right now using this MCU STM32L051C8T6 in a mass production up to 32.000 setsRight now we have met a problem,afer all 32000 pcs have been programmed with an hex file.I was found mcu have been locked and we cannot upload new files into them. 1....

Shullen by Associate
  • 1866 Views
  • 2 replies
  • 1 kudos

Resolved! Strategies for storing SBSFU private key

Hello,We have an STM32 project with SBSFU bootloader used for firmware updates. We have a pipeline that is triggered from GitLab that will compile and sign the firmware and update pakcage. Before taking production private keys into use, we are consid...

sute by Associate III
  • 2061 Views
  • 2 replies
  • 0 kudos

Is it possible to set the option bytes in my firmware?

Hello everyone,I must start a production of PCBA which use the MCU STM32G474QET6 and I need to protect my firmware, I want to set the read protection at Level 1. Is it possible to set that option byte in the firmware when I flash the firmware?Thanks....

AAles.5 by Associate
  • 1504 Views
  • 1 replies
  • 0 kudos