STM32 MCUs Security

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Secure firmware updates from USB Stick on STM32U5 - how to? (2)

@Guillaume K, @Jocelyn RICARD Since my previous question on the same topic (see here) I have reviewed probably all the MCUboot/TF-M-based solutions available for ST MCUs. There are currently four options that I am aware of:TrustedFirmware-M (TF-M) us...

TDJ_0-1709465597599.png
TDJ by Senior III
  • 2248 Views
  • 18 replies
  • 11 kudos

STM32F767IG7x+SBSFU

Running USB virtual serial port program separately is normal,but download the virtual serial program through sbsfu, USB can't recognize it.Can you give me some suggestions,thankyou very much.

Skaix.1 by Associate
  • 343 Views
  • 2 replies
  • 0 kudos

STM32 capabilities

Hi,I would like to move my project to STM32 from another MCU.There are some requirements that I have to comply with and I would like to know if STM32 is a good idea or not.I need to be able to flash the firmware using USB without an USB to UART conve...

STM32F746 USB OTG clock value??

Posted on June 16, 2017 at 12:10Hi,The ProblemI am running uCLinux on the STM32F746. I am using a gadgetfs-based mass storage device with the SD card for a backing file. The USB PHY is an external SMSC ULPI chip. This works fine when connected to mo...