I set the start address about RAM is 0X20002000, and disable shared but execution.Than, I set a function which data is 0x20002004 to change the protected data.when system enter the function, it will reset.
I am using the STM32F746VET6 which was setup with STM32CubeMX project. In the code it creates I see there's a STM32F746VETX_RAM.ld linker file and a #define VECT_TAB_SRAM to locate the IVT in RAM, but I don't see in MX where I specify that I want the...
I have a problem with erasing sector 0 in Bank 1 of a stm32h7 CPU. See my code snipped below...When I run the code in the debugger, the CPU never returns from the call to HAL_FLASHEx_Erase. When I interrupt the programm the PC is set to 0xFFFFFFFE wh...