STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SBSFU with encrypted CBC in KMS?

Hello,We are developing a product based on a STM32WB5MMG. We have configured the SBSFU with OTA (Asymmetric with AES encryption scheme). Everything is working great and I have only one question that came to my mind during the last commit...The CBC ke...

H573 TrustZone Callable Secure Code

Is it possible to call Secure (S) application code from Non-Secure (NS) application code with TrustZone on STM32H573?  I have not seen any examples of this from ST, so I want to know if it is possible or if there is some fundamental reason why not.Th...

DPade.1 by Associate III
  • 1971 Views
  • 2 replies
  • 1 kudos

Continuous reset loop with SBSFU on STM32L4R9. Reset always happens right at the moment the secure engine is called.

When the Secure Engine Call (inside SE_Init() function) is called in this line:e_ret_status = (*SE_CallGatePtr)(SE_INIT_ID, peSE_Status, primask_bit, uSystemCoreClock);(which is between a SE_EnterSecureMode and SE_ExitSecureMode). The MCU resets at t...

0693W00000AP7mlQAD.png
NAhme.2 by Associate II
  • 9719 Views
  • 21 replies
  • 0 kudos

Resolved! SFI

Am searching for SFI documentation without HSM to demonstrate to a Device certificate authority. Can you please share UserManual or ApplicationNote for STM32H573I-DK.BestRegards,P.Hitesh 

AES-GCM Chunk-Size 1

Hello,I'm using AES-GCM using the method cmox_cipher_append() function call, as taken from the example below, taken from Projects\NUCLEO-L476RG\Applications\Cipher\AES_GCM_AEAD_EncryptDecrypt\Src\main.c        retval = cmox_cipher_append(cipher_ctx, ...

Michael1 by Associate
  • 2782 Views
  • 4 replies
  • 3 kudos