2023-03-27 6:12 PM
I complie STM32F769I-Discovery 2_Images demo (SBSFU\Projects\STM32F769I-Discovery\Applications\2_Images\2_Images_UserApp\MDK-ARM) with MDK KEIL 3.37.
If I link project using default UserApp.sct, the packed image is right, and output.txt show below:
block size =16
Magic: b'SFU1'!!
Magic: b'SFU1'!!
number of segment :2
0x8084cb8
number of segment :3
0x80001f8
0x80062e0
Merging
SBSFU Base = 0x8000000
Writing header = 0x8080000
APPLI Base = 0x8080400
Writing to .\\..\\Binary\\\\SBSFU_UserApp.bin 543952But if I modify UserApp.sct to let fw_update_app execute in ITCM
#! armclang --target=arm-arm-none-eabi -mcpu=cortex-m7 -E -xc
; *************************************************************
; *** Scatter-Loading Description File generated by uVision ***
; *************************************************************
#include "..\..\Linker_Common\MDK-ARM\mapping_sbsfu.h"
#include "..\..\Linker_Common\MDK-ARM\mapping_fwimg.h"
LR_ROM (SLOT_ACTIVE_1_START + 0x400) { ; Cortex-M7: align the init vectors on 0x400
vector_start (SLOT_ACTIVE_1_START + 0x400) FIXED VECTOR_SIZE {
*.o (RESET, +First)
}
ROM_region +0 {
*(InRoot$$Sections)
.ANY (+RO)
}
;ITCM 16k
ITCMRAM_region 0x00000200 0x00004000
{
fw_update_app.o (+RO-CODE)
}
SB_RAM_region (SE_REGION_RAM_END + 1) {
.ANY (STACK)
.ANY (HEAP)
.ANY (+RW +ZI)
}
}
; extra ROM region to make sure the binary size is a multiple of the AES block size (16 bytes) and F7 flash writing unit (4 bytes)
LR_ROM1(+0) ALIGN(16) {
ForAlignment +0 {
startup_stm32f769xx.o (ALIGNTOAESBLOCK,+Last)
}
}the packed image is wrong, the output.txt below show that both Writing header and APPLI Base is wrong address.
block size =16
Magic: b'SFU1'!!
Magic: b'SFU1'!!
number of segment :2
0x4b60
number of segment :3
0x80001f8
0x80062e0
Merging
SBSFU Base = 0x8000000
Writing header = -0x200
APPLI Base = 0x200
Writing to .\\..\\Binary\\\\SBSFU_UserApp.bin 134828304
Solved! Go to Solution.
2023-04-16 10:02 PM
Ok, I see thanks.
But, I think that the ITCM is disabled by SBSFU at boot and not mapped with the Memory Protection Unit.
#ifdef SFU_MPU_PROTECT_ENABLE
/**
* @brief Apply MPU protection
* @param uStep Configuration step : SFU_INITIAL_CONFIGURATION, SFU_SECOND_CONFIGURATION, SFU_THIRD_CONFIGURATION
* @retval SFU_ErrorStatus SFU_SUCCESS if successful, SFU_ERROR otherwise.
*/
SFU_ErrorStatus SFU_LL_SECU_SetProtectionMPU(uint8_t uStep)
{
SFU_ErrorStatus e_ret_status = SFU_ERROR;
uint8_t mpu_region_num; /* id of the MPU region being configured */
MPU_Region_InitTypeDef MPU_InitStruct;
/* ITCM address are not mapped by MPU :
* Since an ITCM access can allow a read to SE area
* The ITCM is disabled */
SCB->ITCMCR &= ~SCB_ITCMCR_EN_Msk;So, I think that anyway you will not be able to leverage the ITCM with SBSFU as the secure bootloader unfortunately (as this would break the MPU isolation of the critical bootloader assets).
2023-04-10 1:43 AM
Does someone get this issue?
2023-04-12 1:49 AM
Hi @tercelcn,
can you clarify your use-case?
It seems you want to place the active slot and the active header in ITCM RAM, is this correct?
So, you would:
First, the active image header is a critical asset, I would recommend not exposing it in ITCM RAM as it might be modified in a malicious way.
Secondly, the packed image preparation script expects slots in FLASH.
I think it is confused by the fact that you provide ITCM addresses.
Can you please explain further your needs ?
Thanks & Regards,
Fred
2023-04-16 8:57 PM
I only want to execute CMSIS-2 CODE in ITCM SRAM, not active header. Code below demonstrate that code in fw_update_app will execute in ITCM .
;ITCM 16k
ITCMRAM_region 0x00000200 0x00004000
{
fw_update_app.o (+RO-CODE)
}
2023-04-16 10:02 PM
Ok, I see thanks.
But, I think that the ITCM is disabled by SBSFU at boot and not mapped with the Memory Protection Unit.
#ifdef SFU_MPU_PROTECT_ENABLE
/**
* @brief Apply MPU protection
* @param uStep Configuration step : SFU_INITIAL_CONFIGURATION, SFU_SECOND_CONFIGURATION, SFU_THIRD_CONFIGURATION
* @retval SFU_ErrorStatus SFU_SUCCESS if successful, SFU_ERROR otherwise.
*/
SFU_ErrorStatus SFU_LL_SECU_SetProtectionMPU(uint8_t uStep)
{
SFU_ErrorStatus e_ret_status = SFU_ERROR;
uint8_t mpu_region_num; /* id of the MPU region being configured */
MPU_Region_InitTypeDef MPU_InitStruct;
/* ITCM address are not mapped by MPU :
* Since an ITCM access can allow a read to SE area
* The ITCM is disabled */
SCB->ITCMCR &= ~SCB_ITCMCR_EN_Msk;So, I think that anyway you will not be able to leverage the ITCM with SBSFU as the secure bootloader unfortunately (as this would break the MPU isolation of the critical bootloader assets).
2023-04-17 5:47 AM
Thanks!