cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750IB How set the RDP Level ?

JFieb.1
Associate

When I set the RDP Level 1 the Controller stops working.

I must unpower the Controller and power it agin, NRST didn't work.

I use the code:

       HAL_FLASH_Unlock();

       HAL_FLASH_OB_Unlock();

       OBIni.OptionType = OPTIONBYTE_RDP;

       OBIni.RDPLevel = OB_RDP_LEVEL_1;

       if ( HAL_FLASHEx_OBProgram(&OBIni) != HAL_OK )

       {

          HAL_FLASH_OB_Lock();

          HAL_FLASH_Lock();

          return;

       }

       HAL_FLASH_OB_Launch();

       /* We should not make it past the Launch, so lock

        * flash memory and return an error from function

        */

       HAL_FLASH_OB_Lock();

       HAL_FLASH_Lock();          

What must I do, that the controller didnt stop after the HAL_FLASH_OB_Launch(); ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hello @Jürgen Fiebig​,

Check this article How to program STM32 Option Bytes with the HAL API 2. Setting RDP Level

Note:  HAL_FLASH_OB_Launch(); is called to generate System Reset to load the new option byte values.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL