STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Restart HSM (STM32HSM-V2AE)

Hello,I am following the guide to generate SFI files. I am testing and have programmed the HSM. Is there any way to "restart" the HSM? Is there any way to start the guide over as if I hadn't done anything?I am particularly interested in obtaining inf...

Sin título.png
mikel-m by Associate III
  • 1265 Views
  • 1 replies
  • 0 kudos

STM32U5 TFM mbedCrypto ECDSA(PSA API)

hi i am implementing a TFM based project on stm32u585 microcontroller. i taken reference from the cubeU5 package to implement the TFM code stm32U585 SBSFU  .in my application i need to use the ECDSA signing and verification using the PSA APIs availab...

sabari1_0-1715335327575.png sabari1_1-1715335390727.png sabari1_2-1715335552924.png sabari1_0-1715592513404.png
sabari1 by Associate III
  • 2565 Views
  • 2 replies
  • 2 kudos

Resolved! Firmware with SBSFU bootloader with SFI at manufacturing

Hi,I am doing feasibility on SBSFU bootloader on STM32H753ZI. Currently in our firmware we are planning to have a custom bootloader based on SBSFU for secure boot and update. But I came across SFI feature from ST to ensure protection at the manufactu...

h_adi by Associate
  • 1809 Views
  • 1 replies
  • 0 kudos

ECDH fails for CURVE25519 using X-CUBE-CRYPTOLIB

I can't get ECDH working for CURVE25519 using the STM32 HAL / crypto lib. This may be an issue with the somewhat confusing constants for this library. I can get the NIST curves working with ECDH. The trouble I have is it seems there are two cmox_ecc_...

antfarmer by Associate III
  • 2286 Views
  • 2 replies
  • 0 kudos

Reg Issue in Running TFM Application STM32u585

Hi @Jocelyn RICARD Greetingswe are working on the STM32u585 TFM Application and are facing issues when running the code. the issue is after dumping the code using the TFM_Update.sh script first time every operation is normal, but while running for th...

PJose4_1-1717159815680.png PJose4_0-1717159805665.png PJose4_2-1717159828600.png PJose4_3-1717159836411.png
PJose.4 by Senior
  • 1210 Views
  • 1 replies
  • 1 kudos