STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trusted Firmware-M v2.1.0 - Bricked Nucleo-L552ZE-Q

Hello,I followed this tutorial to add an example secure partition in TF-M ( https://tf-m-user-guide.trustedfirmware.org/integration_guide/services/tfm_secure_partition_addition.html ) and then followed these instructions to flash the application to m...

MCost4_0-1716225932046.png
MCost.4 by Associate II
  • 10645 Views
  • 25 replies
  • 1 kudos

TFM building

 Hello,I am trying to compile the TFM application, but when building the TFM Appli Secure project, it says it cannot find the file tfm_parse_manifest_list.exe and gives me errors because not all the .h files that should be generated by running the pr...

Resolved! Can x-cube-sbsfu use hardware decryption?

I'm using H753 which has hw crypto, and was hoping to improve the sbsfu execution time (e.g. time to validate FW header at start tup) by enabling hw crypto. However HAL_CRYP_MODULE_ENABLED doesn't do anything. I looked through the integration guide a...

JQiao.1 by Associate II
  • 1189 Views
  • 1 replies
  • 0 kudos

Encryption using AES CCM + MIC - stm32wb

Hi,i am trying to develop a device which sends out bthome advertisements via ble (some sensor data).So far so good, this part is working, but now i would also like to use bthome encryption.https://bthome.io/encryption/So following this guide, i would...

Exeu by Associate III
  • 2063 Views
  • 0 replies
  • 0 kudos