STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SBSFU on STM32H743 SWAP_BANK

I am new to SBSFU. I picked the NUCLEO-H753ZI project to try on a board with STM32H743. Everything seems to be running fine but ONLY when the SWAP_BANK is unchecked at startup. When it is checked before flashing, the board doesn't run as it was progr...

starmour by Associate II
  • 5513 Views
  • 8 replies
  • 0 kudos

STM32H563 Warning: The Core is locked up

Hi,I'm currently developing a custom application which provisions and regresses an STM32H563, using the NUCLEO-H563ZI board for development.The CubeProgrammer CLI commands I'm executing are based on the bash scripts generated by CubeMX. Since I start...

Resolved! Are x-cube-cryptolib V.4 cmox_ functions reentrant?

Hi, I planned of implementing this library in a new STM32G4 application. I have no RTOS, and I need to make  cryptographic functions calls from both main loop and interrupts. So, instead of wasting time in building a thread-safe scheduling mechanism ...

mcasoni by Associate
  • 1412 Views
  • 2 replies
  • 1 kudos

Resolved! SBSFU STM32H7 script

Hello,   These are the scripts available for the L4 series, Can the same scripts be used for H7 series MCUs. If not, are there any specific scripts/commands needs to be followed.     Regards,Devank J

image (5).png
Devank_J by Associate II
  • 2246 Views
  • 3 replies
  • 1 kudos