Skip to main content
Visitor II
April 11, 2024
Question

[STM32WB FUS CKS] Is removal of stored keys a planned feature?

  • April 11, 2024
  • 1 reply
  • 905 views

Hello,
I'm struggling to find any information regarding possibility to remove the keys stored through FUS CKS.
My understanding is, if the keys are constantly being stored to some reserved space in flash memory, this reserved space will eventually be full and another key write will be impossible.
I found two related threads with no answer to this problem:
 https://community.st.com/t5/stm32-mcus-security/stm32wb-fus-cks-no-option-to-delete-or-overwrite-userkeys/td-p/586508
https://community.st.com/t5/stm32-mcus-security/how-can-i-wipe-user-key-fus-ws-cks-when-all-index-positions-are/td-p/62762

Is it possible at this point to add key removal to the API? Is such feature planned?

Regards,
Larry

This topic has been closed for replies.

1 reply

ST Employee
April 12, 2024

Hello @larry_g,

Based on the information provided in AN5185 (see section 5.1 Key types and structure), FUS system is designed to store a limited number of keys (101 keys, including 1 master key and 100 clear/encrypted keys), and it is explicitly stated that any stored key cannot be changed or removed. This implies that once a key is written into the FUS, it occupies a slot permanently.

Given this constraint, it is not possible to remove keys once they are stored in the FUS. The reason behind this is to disallow the removal or change of keys for security purposes to prevent tampering with the keys after they have been set.

If the reserved space for keys in the FUS becomes full, no additional keys can be written, and any attempt to write more than the supported number of keys will be rejected with an error message. This must be considered when designing the system that will use the FUS.

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.