STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SBSFU STM32H7 script

Hello,   These are the scripts available for the L4 series, Can the same scripts be used for H7 series MCUs. If not, are there any specific scripts/commands needs to be followed.     Regards,Devank J

image (5).png
Devank_J by Associate II
  • 2343 Views
  • 3 replies
  • 1 kudos

STM32H573xx: update with ST-JLINK

In the case of a root of trust with two boot stages (STiRoT + OEMuRoT), I'm looking to update the OEMuRoT or the firmware. From STM32CubeProgrammer I can do this via the bootloader. However, when I use the ST-LINK probe and try to program the new fir...

failed_to_download_fw.png

Secure H743 firnware programming GUI tools

I've read the X-CUBE-SBSFU Secure Boot and Secure Firmware documents and it doesn't explain if these are tools, with GUI, or just an API, which should really be explained at the start.If you know all about it I am sure these documents are just great,...

Robmar by Senior III
  • 2574 Views
  • 4 replies
  • 2 kudos

Resolved! SBSFU-UserApplication-Debugging

I'm curious what is the best way to debug a User Application when using SBSFU on a STM32.Of course the security mechanisms in SBSFU/SECore must be disabled to allow debugging at all and basically just downloading the UserApplication and debug it with...

STM32H725 - RDP locked to BB

Hello, I have a problem with a STM32H725, the Option byte RDP is locked to the value BB.In fact, I try to change other option bytes and it always fail with this error: " Error: Option Byte Programming failed Or modified by application after OB_LAUNCH...

Dams by Associate III
  • 2309 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.