STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1742 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4891 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9593 Views
  • 5 replies
  • 3 kudos

STM32CubeMX error loading existing project

"Can't Add: MotorControl files not found"This above is the error I get when I try to load an existing project using STCubeMX V5.6.0.My toolchain set up works on my laptop and I attempted to duplicate the same tools on my work computer. Both are Wind...

BTrem.1 by Senior II
  • 1979 Views
  • 4 replies
  • 0 kudos

Resolved! Why are Regular Conversion Manager (RCM) functions not present in the MC SDK 5.4.3 code while present in the documentation?

Hi,I am develloping a system using the motor control sdk. I am usiung the ‎STSPIN32F0‎ chip and the following software versions:This module only has one ADC peripheral and I need to use it in my application. Looking around, I have found that the Regu...

0693W000000Wl3fQAC.png 0693W000000Wl3uQAC.png 0693W000000Wl4YQAS.png 0693W000000Wl4iQAC.png
PBela.1 by Associate II
  • 2936 Views
  • 4 replies
  • 1 kudos

How to measure RPM with STEVAL-ESC002V1?

I succeeded in operating the Tartget Motor with STEVAL-ESC002V1.However, since the STEVAL-ESC002V1 is not linked with'Motor Profiler 5.4.4' SDK, it is impossible to check the motor operating speed.​I know that STSPIN32F0A has a function that can meas...

WSeun.1 by Associate
  • 1996 Views
  • 5 replies
  • 1 kudos

Resolved! Over current protections by pass in steval 3202

hi sir i am using motor control workbench generated foc sdk and running motor of 6 pole bldc successfully but in my application of motor heavy load is given on motor so it indicate over current fault so please guide me to by pass overcurrent fault fr...

Ryada.1 by Associate II
  • 1607 Views
  • 2 replies
  • 0 kudos

Motor becomes unstable at 1200 RPM and stops with the P-NUCLEO-IHM001 Motor control Kit and Motor Control SDK 5.4.4 .

I am using the P-NUCLEO-IHM001 motor development kit Hardware: Microcontroller Board: NUCLEO-F302R8Driver Board: X-NUCLEO-IHM07M1Motor: Bull-Running model BR2804-1700 kVSoftware:Keil uVision 5 IDEST Motor Control Workbench 5.4.4Motor Control SDK 5.4....

0693W000006GNQhQAO.jpg 0693W000006GNRGQA4.jpg
AKhar.3 by Associate
  • 1638 Views
  • 3 replies
  • 0 kudos