STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1729 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9574 Views
  • 5 replies
  • 3 kudos

ST MC workbench Current sense

Posted on September 24, 2015 at 19:54Hi,I am using ST MC Workbench to design a BLDC FOC motor driver, and am running into a problem.  I am using three shunt resistors to sense current (one per channel) and am trying to use ''embedded PGA'' as an amp...

STM Studio - STM32 PMSM FOC LIBv4.2 variables

Posted on October 14, 2015 at 23:54Hi, I am running the STM32 PMSM FOC LIBv4.2, using encoder and I am trying to visualize the variables values through the STM Studio. The variable names used here are the default used in the STM32 PMSM FOC LIBv4.2I ...

cviolino by Associate II
  • 1197 Views
  • 2 replies
  • 0 kudos

ST Motor Control Workbench Under Voltage Fault

Posted on February 18, 2016 at 20:17I'm using the ST Motor Control Workbench with STEVAL-IFN003V1 and my bus voltage is reading above the threshold but the Under Voltage fault light is constantly on even if I disable the low voltage checking in the ...

Konami by Senior II
  • 1437 Views
  • 2 replies
  • 0 kudos

STM3240G recommended Motor kit IHM-???

Posted on March 31, 2016 at 22:03Hi, I am not having much luck with the Nucleo-IHM001 eval kit(s), for now going to put them down, very dissapointing. I have a STM3240G eval board that appears to be supported by the ST motor control workbench. Can a...

Low speed FOC control X nucleo-ihM07m1

Posted on April 21, 2016 at 01:25Hi ,Just a bit of background. We do motion control products and require smooth low speed to high speed motion. We also need high torque and all this lends itself to BLDC and PMSM motors. From the research Ive done it...

imtiaz by Associate II
  • 2971 Views
  • 6 replies
  • 0 kudos

Not enough torque when using MC PMSM FOC Lib 4.2

Posted on May 12, 2016 at 13:53Hello,I am trying to control In-wheel motor for electric scooter. Here is what I have done so far....1. In-Wheel motor : 300W ,   Hall sensor  (Surface Mounted PMSM)2. 3 Shunt phase current sensing3. MC workbench PMSM ...

erenes by Associate II
  • 2912 Views
  • 8 replies
  • 0 kudos

Start-up Failure using FOC lib

Posted on May 14, 2016 at 03:18Hello I try to use In-Wheel motor. 300W with Hall sensor.I used workbench and finally succeeded to run Motor Profiler .And got motor parameters, PID gains.After this, applied these parameters and tried to run the motor...

erenes by Associate II
  • 1093 Views
  • 2 replies
  • 0 kudos

Start up torque

Posted on May 17, 2016 at 11:56Hello,What I have done so far is ...0. In controlling of 300W 24V In-Wheel motor ... (with STM32F407VE)1. Motor parameters were taken through Motor Profiler2. Hall sensor is set to main sensor.  And Observer+PLL is aux...

erenes by Associate II
  • 1066 Views
  • 2 replies
  • 0 kudos

IHM07M1 ST workbench Motor Profile Overcurrent Fault

Posted on July 31, 2016 at 20:13Hi,I have a the P-NUCLEO-IHM001 kit, and having issues completing the motor profile step.Setup:1. keil IDE loading firmware complete, board setup in FOC, 3 shunt jumpers.2. ST workbench profile using example project '...

cchiau by Associate
  • 1034 Views
  • 1 replies
  • 0 kudos