User Activity

Hi,I have a P-NUCLEO-IHM03 dev kit which comes with a iPower gimbal motor (GBM2804 – 100T) , NUCLEO-G431RB and a power shield. I am running the 'Speed Ramp with potentiometer on P-NUCLEO-IHM03 kit' example in the motor control workbench.My intention ...
Hi,I am trying to do six step BLDC commutation on STEVAL-SPIN3202 to control a gimbal motor https://www.robotshop.com/ca/en/ipower-gbm5208h-200t-gimbal-motor.htmlI am using the STSPIN32F0_Uart example under the following sw packagehttps://www.st.com/...
Hi,I have a STEVAL-STSPIN3202 evaluation board and trying to setup the environment on MacOS. When I plug in the eval board with a USB B cable to my MacBook, I don’t see a device in both ls /dev/tty* and ls /dev/cu*No devices even when I do, ioreg -p ...
Kudos from