STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Payload length in Serial Communication in MCSDK

Hi everybody,I read the document UM1052 and in this document we can see this "Payload_Length: the total number of bytes that compose the frame payload". My question is: does the payload length include Payload_length byte itself and CRC ?Precisely wha...

Randy1 by Associate III
  • 1234 Views
  • 2 replies
  • 0 kudos

SVPWM implementation with MCSDK

Hi,I have studied UM1052 user manual about vector control implementation on PMSM. But I have two major problems. The first one is with the SVPWM implementation on sector 4.11 and the other one is "Circle limitation" on sector 4.12.1 .I am actually lo...

Resolved! EVSPIN32F0601S3 + ST Motor Profiler

Hey. When will it be possible to add the EVSPIN32F0601S3 board to the ST Motor Profiler? Or which one to choose from the proposed for determining the parameters of the electric motor?

SLodo.1 by Associate
  • 2082 Views
  • 4 replies
  • 1 kudos

Cant generate project

Hi, firstly I installed java 8 and I installed STM32Cubemx 5.6. after that I installed X-CUBE-MCSDK. But gave message in the setting of the project generation that "STM32CubeMX not found - ver. "5.2.0" or higher is required".

mkk.1 by Associate II
  • 1391 Views
  • 1 replies
  • 0 kudos