cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3201

STEVAL-SPIN3201

I have a motor connected to this board and just cannot get it to run correctly.

I get the start up error or speed feedback error when running the motor.

I am running the motor in sensor less mode using the sample software (SDK5x - STEVAL-SPIN3201 - BullRunning.stmcx) with adjusted parameters.

I get the motor to startup (appears to be correct) but then when it reaches target rpm it the fails (most of the time with startup error)

I am using ST motor control Workbench, STM 32 Cube and IAR

Please can you assist with getting the motor to actually spin.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards