STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1693 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4847 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9525 Views
  • 5 replies
  • 3 kudos

Resolved! ADC not working with NUCLEO-G431RB.

NUCLEO-G431RB + X-NUCLEO-IHM07M1MCWB 5.Y.3 + STM32CubeIDE 1.7.0Maxon motor combination: 200142 + 166935 + 673026I have created a project to drive a BLDC motor with the above mentioned equipment, I was able to create a basic project to drive the ...

msingh by Senior
  • 3106 Views
  • 3 replies
  • 0 kudos

Whitepaper - Improve Motor Drive Efficiency

Check our recent whitepaper on how to improve motor drive efficiency Register here and read through the latest techniques:Optimized AC inverter designsChoice of the inverter switching frequencyPWM modulation techniquesSoftware Control methods for ens...

0693W00000FBLrSQAX.png

Oscillation at higher load in Speed mode

Ian using a dyno to apply load and using B-G431B-ESC1 with a pmsm motorSPEED: KI= 950, KP= 13767, Torque KI= 1005 reduced from 3005 earlier torque kp=82 (tuned settings)I have attached a snapshot ,as gradually I increase load (oz-in) in steps1) at rp...

Ajosh.1 by Associate
  • 1809 Views
  • 1 replies
  • 0 kudos

Can you help me for (Are there videos for the starting guide for the STM3210B-MCKIT PMSM starter control kit?

I have STM3210B-MCKIT PMSM starter control kit, It is worked through LCD and for start and stop the motor.but I would like to develop a new controller and change the control system. I would like to a guide and If there is a library that has the proje...

ADiab.2 by Associate
  • 1216 Views
  • 1 replies
  • 0 kudos

Why is ESC not starting the DC motor?

Hi, I am using the code below to spin my brushless DC motor. When I used another code where I have a potentiometer to vary the motor speed, the motor spins without problem so I don't think the DC motor and ESC are faulty. Is there something wrong wit...

M7890.1 by Associate III
  • 1559 Views
  • 1 replies
  • 0 kudos

Resolved! How to measure the motor parameter?

 Is st mc sdk support measure the motor parameter only use the board, not use STMotorProfiler?It is useful to driver different motor when the foc board used as a general driver product.

llm by Associate III
  • 1341 Views
  • 1 replies
  • 1 kudos

how and where to download the st foc example source code?

I mean the eval board foc source code., not the sdk. I searched on the st website, but find none.In the pc directory "STMotorProfiler\resources\assets\fws", I found the firmware, like as NUCLEO-F446RE#STEVAL-IPMNG3Q 3Sh#(5.4.0)#(3A1B794F).hex, but I...

llm by Associate III
  • 1195 Views
  • 1 replies
  • 1 kudos

Problem with correct value of placement electrical angle in MC and smooth movement in both directions (Torque mode + HALL sensors)

Hi,I have one TMOTOR RI-70 KV95 BLDC motor with HALL sensors and harmonic grive gear 1:120 and payload 10Nm controled by evalkit NUCLEOG431+X-NUCLEO-IHM08M1. I need to control it in torque mode.I generate application in MotorControl 5.4.6, FW 1.1. Wi...

ketchup by Associate III
  • 1503 Views
  • 2 replies
  • 0 kudos