2018-11-27 7:42 AM
When will the HF-Injection feature be enabled for the MCSDK_v5.x.x?
I figured out, that it has been enabled in the v4.3, but in v5.2 it is only declared as "Available in a later release". Is there a possibilty to estimate a date, when this feature will be enabled?
Thanks for your answer.
2018-11-29 2:44 AM
Dear Luca,
We decided not to port the HFI in the MCSDK5.x. Indeed it works only with a limited number of motors. We are now thinking to replace HFI by a new algorithm. It will not be available before end 2019. Sorry for the inconvenience,
Best regards,
Claire
2018-11-29 2:17 PM
Hallo Claire,
thank you for your answer.
Ist there a other method to achieve standstill torque with the X-CUBE-MCSDK?
If it's possible sensorless.
Kind regards,
Luca
2021-06-27 10:26 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards