STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F767zi - MX_LWIP_Process()

Hello,I just started working with STM32f767zi board. I'm doing TCP Ethernet communication using lwip RAW API. I could be able to start the communication with the host. But the problem is, in my forever loop I put MX_LWIP_Process() function. If I put ...

KMale.1 by Associate II
  • 3118 Views
  • 5 replies
  • 0 kudos

USB MSC SRAM is not working

I am using stm32f072rb discovery board... I want to use SRAM as mass storage... I am attaching the project... I am getting the memory on windows but on the format it shows an error like "windows is unable to format".

Ethernet - RMII vs MII

I'm working on an application that requires Ethernet on an STM32F765 chip and there are two options to attach an Ethernet PHY to the MCU: RMII and MII. Deciding on which interface to use has led me to a post that mentioned RMII having issues on STM32...

ARoth.1 by Associate II
  • 16893 Views
  • 6 replies
  • 0 kudos

LWIP: MEMP_SYS_TIMEOUT could not be resolved

Hi,I'm trying to compile my project that uses Ethernet interface. I have a PCB with STM32F407VGT6. When I compile, I get 3 errors that say: MEMP_SYS_TIMEOUT could not be resolved. The error is located at timeouts.c file, in lwip library.These are:tim...

JCOrtiz by Associate II
  • 1134 Views
  • 0 replies
  • 0 kudos

Nucleo-H743zi2 + freeRTOS, TIM4 PWM doesn't work!

I'm using nucleo-h743zi2 with freeRTOS for drone flight controller projectbefore using h743, I tested my code on f429zi everything works fineBut after migrate to h743, All PWM channels on TIM4 does't work,Prescaler and counter period is correct for 5...

Cyeoj.1 by Associate
  • 3298 Views
  • 6 replies
  • 0 kudos

Hello ! I want to use a MIDI interface with my stm32 board. I found some codes but so complex that I failed to extract what I wanted. Does anyone know how to do a simple MIDI communication ?

I have two boards, STM32F303K8 and STM32F411RE, and I'm using the HAL librairie with CubeIDE 1.3.1. I don't know if these information are useful but we never know...If my question lacks information, do not hesitate to ask me what is missing in my que...

GMich.2 by Associate II
  • 4152 Views
  • 5 replies
  • 1 kudos

Basic UCPD Sink on STM32G071CBU6

Hi,I am following your guides for the simple USB-PD Sink from here:https://www.st.com/resource/en/application_note/dm00663511-how-to-build-a-simple-usb-pd-sink-application-with-stm32cubemx-stmicroelectronics.pdfand here:https://www.youtube.com/watch?...

0693W000003Pp7jQAC.jpg
IHend.1 by Associate II
  • 3386 Views
  • 6 replies
  • 0 kudos

TIM2 with RTOS PeriodElapsCallback executed once only

Hello,I have a simple project. I'm using FreeRTOS and programmed TIM2 1ms interrupt.The TIM2_IRQHandler and PeriodElapsCallback are only called once in the beginning but not after.I set Clock at 64MHz, the PSC is 63999 and Counter period is 9 I expe...

CSand by Associate III
  • 1887 Views
  • 3 replies
  • 0 kudos