STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PWM pattern changed after fixed no of cycles

Hi everyone,I am trying to generate sinewave using PWM mode of microcontroller.I am using Discovery Board having STM32F407 microcontroller. System clock and Timer clock are of 8MhzI am using two timers Timer1 for High Frequency switching (500Hz) and ...

PWM_response.jpg
AHayee by Associate II
  • 658 Views
  • 6 replies
  • 2 kudos

STM32H7S7 USB Webcam driver

Hi,We are currently using STM32H7S7 MCU with display and similar USB C circuit from the developer board.I wanted to connect a Web camera and to be able to display video from the screen.I wanted some help and guidance on where to find the driver?does ...

ropodi17 by Associate II
  • 385 Views
  • 1 replies
  • 0 kudos

issue of ThreadX and FDCAN function

Hello @D.Botelho @mƎALLEm  I had an issue of ThreadX and FDCAN transmit as below. I use the stm32g474 and config a threadx and fdcan with stm32cubemx, so far it works well. but when i add some fdcan transmit code, it comes strangely. the code as belo...

dqsh06 by Senior
  • 1121 Views
  • 11 replies
  • 0 kudos

Resolved! Update the color config for the VD66GY sensor

 Hello,On the STM32N6, I am using DCMIPP_PIXEL_PACKER_FORMAT_YUV422_1.I am seeing the correct coloring when using CMW_MIRRORFLIP_NONE and the incorrect coloring when setting CMW_MIRRORFLIP_FLIP. Any help getting the correct DCMIPP_ColorConversionConf...

FB__1 by Associate III
  • 747 Views
  • 1 replies
  • 0 kudos