STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I try to communication with two stm32f4 via CAN bus. the first board (which transmit the message) as can1 and the second (which receive the message) as can2. I'm using the new HAL_CAN function.

In polling mode, HAL_CAN_AddTxMessage() returns HAL_OK, but HAL_CAN_GetRxMessage() returns HAL_CAN_ERROR_PARAM. In interrupt mode, the function HAL_CAN_RxFifo0MsgPendingCallback() never has been called (CAN1_RX0_IRQHandler not been called). Also HAL...

AS.5 by Associate II
  • 3646 Views
  • 5 replies
  • 0 kudos

Windows Driver/INF files for ECM

Hi there,Windows does not contain a default ECM driver like Linux does. I was wondering if there was any intention providing a Windows driver for the ECM middleware that is in the framework? We have to work with specific Android phones, which do no...

JKaz.1 by Associate III
  • 749 Views
  • 1 replies
  • 0 kudos

PDM2PCM Library will not link.

Hi.I'm working on a STM32F4-Discovery board, and I'm having trouble linking the PDM2PCM Library into my project. I have run the example project located in the STM32F4-Discovery folder called "Audio_playback_and_record" and it works fine.I have copied...

0690X00000Aq089QAB.jpg
mbmail4 by Associate II
  • 2344 Views
  • 2 replies
  • 0 kudos

USBPD message sequence issue.

Hi STteam,@brief : We are working PD source solution(i.e. 60Watt (20V @ 3A max)) using STM32G081RBT6. We are taking USB-PD_Provider_1port as an Base reference project.@Reference : I have gone through each and every line of UM2552 reference manual I f...

HGorl.1 by Associate II
  • 1194 Views
  • 1 replies
  • 0 kudos

Issues with SD Card when waiting for SD Card Ready

Hi everybody,I've got an STM32H743XI and use the Cube V1.3.2 Firmware for an project for my master thesis.To this controller I have connected a SD Card with the SDMMC controller using the 4 bit bus. I also use FreeRtos and don't want a blocking read ...

maxmax1 by Associate
  • 1764 Views
  • 2 replies
  • 1 kudos