STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bug in Low-Level driver LL_SPI_ReceiveData8 for STM32L0, STM32L4, STM32L5 and possibly others

Affected driver libraries: STM32Cube_FW_L5_V1.4.0, STM32Cube_FW_L4_V1.16.0, STM32Cube_FW_L0_V1.11.2 and possibly other device driver libraries based on the same SPI peripheralFile: stm32yyxx_ll_spi.h (Replace yy by L5, L4, F0, ...)Functions affected:...

SOfne.1 by Associate III
  • 3636 Views
  • 6 replies
  • 0 kudos

USB HID REPORT DESCRIPTOR SIZE

I have a report descriptor that consist of 456 bytes. The problem is : When i define USBD_CUSTOM_HID_REPORT_DESC_SIZE   456 in usbd_conf.h file, it raises overlow warning and my hid device no longer works. How can i define hid descriptor size bigge...

TDuma.1 by Associate
  • 1521 Views
  • 2 replies
  • 1 kudos

STM32F070F6 Bootloader USB DFU Mode not working.

I want to use STM32F070F6 usb dfu mode to upload program. The document An2606 page 53 says:If HSE is present and has a value of 24, 18, 16, 12, 8, 6, 4 MHz, the system clock is configured to 48 MHz with HSE as clock source. The DFU interface, USART1,...

0693W000001sOCMQA2.jpg
TYu.1951 by Associate II
  • 1927 Views
  • 2 replies
  • 0 kudos
ASpar.1 by Associate II
  • 3042 Views
  • 5 replies
  • 0 kudos

Resolved! Hardfault with Lwip Udp

Hello, I'm having trouble about use of lwip on Stm32h743. I'm using udp raw. I'm transmitting packet with 1ms period, there is no problem in sending/receiving. After 20-30 min, program is going to hardfault with 'Imprecise data access violation'. It ...

0693W000008xdWuQAI.png
Ey.1 by Associate II
  • 4095 Views
  • 6 replies
  • 0 kudos