cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a bug in the SVD file for the STM32G431?

frank
Associate II

Is there a bug in the SVD file for the STM32G431? It appears to list ADC12_Common->CCR as being at address 0x50000208 when it supposed to be at 0x50000308

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen GH
ST Employee

Hello @frank​ ,

This issue is already detected and under resolution

Regards

frank
Associate II

Can you also please check the CPAC and SCB definitions.

Hi @frank​ ,

Please note that the SCB iissue i reported internally, following this request: https://community.st.com/s/question/0D53W000004IkPuSAK/most-up-to-date-svd-for-stm32g474.

For CPACR and ADC_COMMON base addresses: they are already fixed in internal version of SVD files that will be available soon on the web and deployed for the IDEs.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.