STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hi, I am using FREE RTOS on STM32F429. Facing "Data read write issue" in internal SRAM Memory address. Need help.

I had created single task with normal priority. The task has three functions. In one function ,I am writing the 2 byte data into internal SRAM (starting address for e.g. 0x20010204) .The 2 byte data is written on memory addresses 0x20010204 and 0x200...

ADank.2 by Associate II
  • 1564 Views
  • 3 replies
  • 0 kudos

STM32L496 - DFU Exit detection

Hello, I'm running into a bit of trouble updating firmware using DFU. This would not be such a big deal, apart from the fact that sometimes an upgrade needs to be made without the ST-Link tool.First of all, entering DFU mode and re-flashing the firmw...

0693W00000Bb5nQQAR.png
AFahr.1 by Associate III
  • 2537 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F072xB GPIO issue | USB pins do not work as GPIO

Hi all,First some context:I am attempting to use the USB designated pins (PA11 and PA12) as generic GPIO inputs at start-up as a way of determining if a host is connected to the device and make a decision whether to run the main code or not - I will ...

JCame.1 by Associate III
  • 7323 Views
  • 15 replies
  • 0 kudos

Resolved! How to update FATFS on STM32F103 Package ?

Hi to all,I need to update from FatFS from R0.11 to R0.12cIn R0.12c there are new implementations compared to 0.11.I see that for the STM32F401 the FATFS is in version 0.12c.Is there a way to update the library for the STM32F103 as well?Thank you.

ABatt.1 by Senior
  • 1823 Views
  • 2 replies
  • 0 kudos