STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! INA226

Hi there!I start to work with this sensor and i want use this functionHAL_I2C_Mem_Write_IT(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress,uint16_t MemAddSize, uint8_t *pData, uint16_t Size)so the pointer address register of the sen...

SGian.1 by Senior
  • 348 Views
  • 2 replies
  • 0 kudos

USB Printer with STM32

How would I go about implementing a USB host for a usb printer. I would like to send things through my STM32 to be printed. I’ve seen adaptations or some work done on the USB printer class as a device but I am unsure how I would do this as a host? An...

Resolved! STM32Cubeide 2.0

Hi there!i start one of my new project with STM32cubeide 2.0. First i start with configure mu MCU in STM32CUBEMX in this casa STM32G031K8T6 afther i configurate all pin i create a poject . So afther i import my project in STM32CubeIde 2.0 and i build...

SGian.1 by Senior
  • 466 Views
  • 4 replies
  • 0 kudos

Resolved! Bugs in sd_diskio.c alignment handling

I've had problems with sd_diskio.c used for SD card I/O with FatFs.CubeMX version is 6.16.0.I'm using SDMMC with DMA, so consideration needs to be given to cache coherency and alignment.I have both these set:#define ENABLE_SD_DMA_CACHE_MAINTENANCE  1...

USB device not recognized with RNDIS using USBX

Hello,I am trying to get Ethernet-over-USB working on a STM32U585. I want to be able to use both RNDIS and CDC-ECM, but I decided to start with RNDIS first. After a lot of trial and error and research, I am running out of ideas as to why my PC does n...

KoCT by Associate II
  • 504 Views
  • 1 replies
  • 0 kudos