STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBD_CDC_ACM_Activate() never get called

Hi,I have implemented CDC USB device on my custom board using STM32C071CBT6. When i connect USB cable to host PC then I can see Virtual COM Port on PC as 'USB Serial Device (COMxx)' However, I tried transmitting some data which I could not receive on...

PPate.1 by Associate III
  • 1534 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H743 Timers + ADC + DMA

Hi you all,as a breef summary; I set up a timer to trigger an adc that should than use the DMA to transfer the data to memory, i need 111 samples at a time. Sadly for some reason this only works for one sample so if i check  __HAL_DMA_GET_COUNTER(g_h...

ICT_TAN_0-1768226675241.png ICT_TAN_1-1768226694036.png ICT_TAN_2-1768226722687.png
ICT_TAN by Associate
  • 465 Views
  • 2 replies
  • 1 kudos

NUCLEO-F401RE + x-cube-ble1: Hard Fault

I’m attempting to learn BLE and IoT and have purchased the following boards to get started.NUCLEO-F401RE    MCU brdX-NUCLEO-IDB05A2  BLE Expansion brdDownloaded:STM32CubeIDE Version: 2.0.0 Build: 26820_20251114_1348 (UTC)STM32CubeMX Version: 6.16.1x-...

Thread safety of code generated by Cube

Hello,I'm wondering if Cube's generated code for is thread safe. In particular, whether malloc can be safely used in a multi-threaded FreeRTOS setup.The broken malloc behavior was first described by Dave Nadler in 2019 here. He has also written about...

unturned3 by Associate II
  • 4680 Views
  • 10 replies
  • 2 kudos

CAM-16GZ driver

I'm using STM32N6 with stm32-mw-camera to communicate to CAM-66GY sensor. I also have CAM-16GZ sensor, but looks like this sensor is not supported (because of VD6G_BAYER_NONE when I use vd6g driver). What are my options to integrate CAM-16GZ into the...