2026-01-06 10:05 AM
I've had problems with sd_diskio.c used for SD card I/O with FatFs.
CubeMX version is 6.16.0.
I'm using SDMMC with DMA, so consideration needs to be given to cache coherency and alignment.
I have both these set:
#define ENABLE_SD_DMA_CACHE_MAINTENANCE 1
#define ENABLE_SCRATCH_BUFFER
However, I've found some bugs in the code:
In SD_read, the alignment check:
#if defined(ENABLE_SCRATCH_BUFFER)
if (!((uint32_t)buff & 0x3))
{
#endif
should have the 0x3 changed to 0x1f, as cache alignment requires 32-byte alignment, not 4-byte.
There's another case of this in SD_write.
Furthermore, there's a bracketing problem in SD_write with the code under ENABLE_SCRATCH_BUFFER conditional compilation, which is supposed to be invoked when the buffer is misaligned as an else condition for if (!((uint32_t)buff & 0x1f), but is instead an else condition for a DMA success check. This means that the scratch buffer code does not run at all when a buffer misalignment is detected.
To fix it, I added a closing brace to this code (lines 488-491)
#if defined(ENABLE_SCRATCH_BUFFER)
+ }
else {
/* Slow path, fetch each sector a part and memcpy to destination buffer */
and deleted the closing brace from this code (lines 556-561):
if ((i == count) && (ret == MSD_OK ))
res = RES_OK;
- }
}
#endif
May I request that these are fixed in the template code? The indentation and conditional compilation are quite a mess, which I'm sure led to the latter problem, so perhaps reformatting and commenting the closing braces and #endifs would be beneficial for maintenance.
Regards,
David
Solved! Go to Solution.
2026-01-06 10:44 AM - edited 2026-01-06 10:44 AM
Can you include your IOC file? I don't see the issues you mention in code generated for the STM32H743. The GitHub mentions some of these issues and says they have been fixed years ago. It's possible you're generating code with an old version.
"0x3" doesn't appear anywhere in the generated sd_diskio.c and it seems like the generated code is correct here (0x1F instead of 0x3):
The file only has 520 lines so I'm unable to compare lines 556-561.
2026-01-06 10:44 AM - edited 2026-01-06 10:44 AM
Can you include your IOC file? I don't see the issues you mention in code generated for the STM32H743. The GitHub mentions some of these issues and says they have been fixed years ago. It's possible you're generating code with an old version.
"0x3" doesn't appear anywhere in the generated sd_diskio.c and it seems like the generated code is correct here (0x1F instead of 0x3):
The file only has 520 lines so I'm unable to compare lines 556-561.
2026-01-07 6:26 AM
I've attached my IOC file.
Seems I'm on FW_H7 V1.11.2 - a version from March 2024.
I tried updating to V1.12.1, and the sd_diskio.c does have the bugfixes.
It also rearranges HAL code directories and breaks my build, which I haven't got time to fix right now. But, looks like the SD card driver has indeed been fixed.