cancel
Showing results for 
Search instead for 
Did you mean: 

USBD_CDC_ACM_Activate() never get called

PPate.1
Associate III

Hi,

I have implemented CDC USB device on my custom board using STM32C071CBT6. When i connect USB cable to host PC then I can see Virtual COM Port on PC as 'USB Serial Device (COMxx)' However, I tried transmitting some data which I could not receive on PC side. After debugging I noticed that function USBD_CDC_ACM_Activate() is never getting called. 

In file, app_usbx_device.c, function MX_USBX_Device_Init() has following code:

UINT MX_USBX_Device_Init(VOID)

{

UINT ret = UX_SUCCESS;

UCHAR *device_framework_high_speed;

UCHAR *device_framework_full_speed;

ULONG device_framework_hs_length;

ULONG device_framework_fs_length;

ULONG string_framework_length;

ULONG language_id_framework_length;

UCHAR *string_framework;

UCHAR *language_id_framework;

 

UCHAR *pointer;

 

/* USER CODE BEGIN MX_USBX_Device_Init0 */

 

/* USER CODE END MX_USBX_Device_Init0 */

pointer = ux_device_byte_pool_buffer;

 

/* Initialize USBX Memory */

if (ux_system_initialize(pointer, USBX_DEVICE_MEMORY_STACK_SIZE, UX_NULL, 0) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_SYSTEM_INITIALIZE_ERROR */

return UX_ERROR;

/* USER CODE END USBX_SYSTEM_INITIALIZE_ERROR */

}

 

/* Get Device Framework High Speed and get the length */

device_framework_high_speed = USBD_Get_Device_Framework_Speed(USBD_HIGH_SPEED,

&device_framework_hs_length);

 

/* Get Device Framework Full Speed and get the length */

device_framework_full_speed = USBD_Get_Device_Framework_Speed(USBD_FULL_SPEED,

&device_framework_fs_length);

 

/* Get String Framework and get the length */

string_framework = USBD_Get_String_Framework(&string_framework_length);

 

/* Get Language Id Framework and get the length */

language_id_framework = USBD_Get_Language_Id_Framework(&language_id_framework_length);

 

/* Install the device portion of USBX */

if (ux_device_stack_initialize(device_framework_high_speed,

device_framework_hs_length,

device_framework_full_speed,

device_framework_fs_length,

string_framework,

string_framework_length,

language_id_framework,

language_id_framework_length,

UX_NULL) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_DEVICE_INITIALIZE_ERROR */

return UX_ERROR;

/* USER CODE END USBX_DEVICE_INITIALIZE_ERROR */

}

 

/* Initialize the cdc acm class parameters for the device */

cdc_acm_parameter.ux_slave_class_cdc_acm_instance_activate = USBD_CDC_ACM_Activate;

cdc_acm_parameter.ux_slave_class_cdc_acm_instance_deactivate = USBD_CDC_ACM_Deactivate;

cdc_acm_parameter.ux_slave_class_cdc_acm_parameter_change = USBD_CDC_ACM_ParameterChange;

 

/* USER CODE BEGIN CDC_ACM_PARAMETER */

 

/* USER CODE END CDC_ACM_PARAMETER */

 

/* Get cdc acm configuration number */

cdc_acm_configuration_number = USBD_Get_Configuration_Number(CLASS_TYPE_CDC_ACM, 0);

 

/* Find cdc acm interface number */

cdc_acm_interface_number = USBD_Get_Interface_Number(CLASS_TYPE_CDC_ACM, 0);

 

/* Initialize the device cdc acm class */

if (ux_device_stack_class_register(_ux_system_slave_class_cdc_acm_name,

ux_device_class_cdc_acm_entry,

cdc_acm_configuration_number,

cdc_acm_interface_number,

&cdc_acm_parameter) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_DEVICE_CDC_ACM_REGISTER_ERROR */

return UX_ERROR;

/* USER CODE END USBX_DEVICE_CDC_ACM_REGISTER_ERROR */

}

 

/* USER CODE BEGIN MX_USBX_Device_Init1 */

 

/* Initialization of USB device */

USBX_APP_Device_Init();

 

/* USER CODE END MX_USBX_Device_Init1 */

 

return ret;

}

 

VOID USBX_APP_Device_Init(VOID)

{

/* USER CODE BEGIN USB_Device_Init_PreTreatment_0 */

 

/* USER CODE END USB_Device_Init_PreTreatment_0 */

 

/* USB_DRD_FS init function */

MX_USB_PCD_Init();

/* USB_DRD_FS init function */

 

 

/* USER CODE BEGIN USB_Device_Init_PreTreatment_1 */

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x00, PCD_SNG_BUF, 0x0C);

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x80, PCD_SNG_BUF, 0x4C);

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x81, PCD_SNG_BUF, 0x8C);

/* USER CODE END USB_Device_Init_PreTreatment_1 */

 

/* Initialize the device controller driver*/

ux_dcd_stm32_initialize((ULONG)USB_DRD_FS, (ULONG)&hpcd_USB_DRD_FS);

/* Start the USB device */

HAL_PCD_Start(&hpcd_USB_DRD_FS);

 

/* USER CODE BEGIN USB_Device_Init_PostTreatment */

 

/* USER CODE END USB_Device_Init_PostTreatment */

}

 

Is something wrong in above init code? Please help locating the issue.

Thanks,

Pradeep

1 ACCEPTED SOLUTION

Accepted Solutions
PPate.1
Associate III

This problem is resolved using USB Classic library instead of USBX.

https://community.st.com/t5/stm32-mcus-embedded-software/usbx-standalone-example-for-cdc-acm/m-p/790010#M61898

More details on above link.

Thanks,

Pradeep

View solution in original post

3 REPLIES 3
PPate.1
Associate III

This problem is resolved using USB Classic library instead of USBX.

https://community.st.com/t5/stm32-mcus-embedded-software/usbx-standalone-example-for-cdc-acm/m-p/790010#M61898

More details on above link.

Thanks,

Pradeep

What, why does this not work on USBX instead? I'm trying to use ThreadX for my application.

r_fujita
Associate

I ran into the same problem and managed to fix it.
I ran into this while using CubeMX. Try increasing UX_MAX_SLAVE_INTERFACES and UX_MAX_DEVICE_INTERFACES.
You can see this by single-stepping through the code, but even when an error occurs, the upper layers don’t get any information about what kind of error it was. Since the error doesn’t propagate properly, there’s no way to retrieve it, which makes this issue particularly hard to debug.

# This was translated using machine translation.